(0)| 7/22/2011 11:19 PM | |
|
Posts: 2 Rating:
|
HELP – IBS Tool Access We wonder if it is of public knowledge, but whether or not, we believe it is important to publish this information that is going to be of great help to power systems engineers or anyone involved in the wide world of electrical protections. Seems weird and illogical but this information is not clearly explained within the pages of Siprotec numerical protection relays' manuals or commissioning documents. Because of this, we think it is our duty to share the information acquired through lab testing experiences. The information which we are going to share is the way to access to IBS tool. In the rush to find relevant data to access this tool we found this useful link: http://siemens.siprotec.de/download_neu/applications/tipps+tricks/Schutz/IBS_WebMon_XP_en.pdf Is important to stress out that this link was obtained after a deep search on internet, though we think it should be published on the manuals or at least be easy to find with just a few keywords. After strictly following the steps described by the document, we couldn't get any positive result. So we got to do some trial and error tests. We ought to correct the following directions: 1.Modem Installation a.When installing the modem, we didn't do it with the speed recommended by the pdf link (couldn't' obtain successful results when installing a 28000 bps modem), but the speed recommended by the "DIGSI 4" disc, which is 33600. see attachment picture 1.jpg b.Following the installation, when the moment comes to select the COM port, is not important which one you choose. But, the port chosen will always be the port in which the data transfer between the Siprotec relay and the computer will be carried out. see attachment picture 2.jpg c.When configuring the port speed, the one which should be selected is the operation interface's and not the service interface's speed. Example:for the Siprotec relays 7UT6** the operation's speed is 57600 and for the Siprotec relay 7SD is 115200. see attachment picture 3.jpg 2.Configure Network Connection a.When writing the username and password, the full access password "000002" for the relay should be entered. see attachment picture 4.jpg b.In the modem configuration window, the speed that we've already set in the modem installation step must be entered, in other words the operation interface's speed of the Siprotec relay. see attachment picture 5.jpg c.If everything has been done right, we can establish a connection with the protection relay. Though, in order to access the web monitor, we've got to obtain its IP address, which in our case was: 192.168.1.1. This address should be written in our favourite web browser, but it should have the latest Java version installed to work properly. see attachment picture 6.jpg d.Enter the IP on the web browser, and enjoy the benefits that this useful tool can provide, which in our concept should be integrated in the DIGSI software. Authors: EGSV (EC) IRVC (EC) [b]Ayuda - Acceso a Herramienta IBS (Siemens)[/b] No sabemos si es de conocimiento general, pero creemos que no esta de mas si anadimos a este foro, cierta información que les va a ser util a otros Ing. en Potencia u otras personas involucradas en el amplio mundo de las protecciones eléctricas. Parece raro pero la siguiente información no esta claramente explicada dentro de los manuales de puesta en servicio de los relés de protección numéricos Siemens-Siprotec, es así que nos vemos en la obligación de compartir esta información obtenida a través de experiencias de pruebas en laboratorio. La información a divulgar es la forma de acceso a la herramienta IBS (IBS Tool). En el afán de búsqueda para poder acceder a esta herramienta pudimos encontrar el siguiente link: http://siemens.siprotec.de/download_neu/applications/tipps+tricks/Schutz/IBS_WebMon_XP_en.pdf Cabe resaltar que este link lo obtuvimos luego de realizar una búsqueda profunda, la cual debería ser de conocimiento público y ser sujeta a poder ser encontrada con unos cuantos keywords o al menos ser publicada en los mismos manuales. Luego de seguir los pasos que constan en dicho documento, no obtuvimos resultados positivos. Por lo tanto tuvimos que realizar ensayos de prueba y error. Debemos corregir los siguientes puntos: [b]1. Modem Installation[/b] a. Al instalar el modem, no lo instalamos con la velocidad que recomienda el archivo PDF (ya que con la velocidad de 28800 bps no obtuvimos resultados satisfactorios), sino con el que recomienda el instalador de aplicaciones que se encuentra en el disco “DIGSI 4”, que es de 33600 bps. see attachment picture 1.jpg b. Al seguir con la instalación, al momento de seleccionar el número del puerto de comunicaciones, debemos recalcar que no es de importancia el número del mismo. Sin embargo, el puerto escogido será siempre el puerto físico en el cual se realizara la transferencia de datos entre el relé y la computadora. see attachment picture 2.jpg c. Al momento de configurar la velocidad del puerto, se deberá ingresarse la velocidad del interfaz de operación y no la velocidad de servicio. Ejemplo: en el relé 7UT6** la velocidad de operación es de 57600, en el relé 7SD es 115200. see attachment picture 3.jpg [b]2. Configure Network Connection[/b] a. Al momento de setear el username y password hay que escribir en el campo password, las clave de acceso completo del relé que es 000002. see attachment picture 4.jpg b. Al momento de estar en la ventana de “modem configuration”, hay que poner la velocidad que ya pusimos en los pasos de modem installation, es decir la misma velocidad de operación del relé. see attachment picture 5.jpg c. Si todo lo hemos hecho de manera adecuada, en estos momentos podemos establecer la conexión con el relé de protección. Sin embargo para poder acceder al navegador del relé, debemos obtener primero tener la dirección IP del mismo; que en nuestro caso fue: 192.168.1.1. Esta dirección IP debemos escribirla en nuestro navegador de internet favorito, sin embargo el navegador debe tener la ultima versión Java disponible en internet e instalada en el ordenador. see attachment picture 6.jpg d. Ingresar el IP en el navegador y listo, podemos acceder a las bondades de esta herramienta, [b]que para nuestro concepto se debería poder acceder directamente a él desde el DIGSI.[/b] [b]Autores:[/b] EGSV (EC) IRVC (EC) Attachmentpictures.zip (552 Downloads) |
Last edited by: O_Moderator at: 8/25/2011 1:23 PMpictures transferred to attachment Last edited by: batusai18 at: 7/23/2011 3:30 PM |
|
| 7/26/2011 10:30 AM | |
|
Joined: 10/9/2007 Last visit: 1/21/2026 Posts: 1295 Rating:
|
Hi Thanks for your information.
The link to this document you can find in www.siprotec.com , under Applications, click on Tips & Trics. Take a look at the pictures attached. Maybe you had problems because you are using an old version of Digsi? In the newer versions you can easily set the IP Address for each serial port. Mike AttachmentIBS Tools.zip (654 Downloads) |
|
Energy Automation products: Sicam, Siprotec, Digsi |
|
| 8/12/2011 12:26 AM | |
|
Posts: 2 Rating:
|
What i was trying to stablish is that the info provided by Siemens was wrong and explain what i did in order to get the IBS tool working. By the way, the moment i added the pictures i could visualize them with no complication, but because a friend of mine warned me about the pictures not being there i decided to add the links to see them. Any other help on how to add images and attachments would be appreciated. PS: it wasnt a digsi version issue, 'cause i'm working with a not so old 4.82 version. |
| 12/2/2016 3:43 PM | |
|
Posts: 1 Rating:
|
Hi! This tool is available for Windows 7? Tnks! |
Follow us on