12/14/2016 11:24 PM | |
Joined: 7/11/2014 Last visit: 7/13/2024 Posts: 4 Rating:
|
I'm using TIA Portal 13 WinCC and I would like to be able to dynamically change the shape of an object, e.g. I need a line of a certain length and by setting a bit I want it to become longer Here are the specs: TIA Portal V13 SP1 Update 9 WinCC Advanced V13 SP1 Update 9 Panel is TP1900 Comfort V13.0.1.0 In the attached screen shot I have one station in the two different situations I want to choose between and if this is possible it will be much more complex than that, but will be simplified greatly if what I want to do is possible. Thanks again, hopefully I have submitted enough information. AttachmentLaGaffe_WinCC_TIA.xlsx (83 Downloads) |
Follow us on