12/19/2016 10:25 AM | |
Joined: 8/3/2009 Last visit: 7/5/2024 Posts: 13231 Rating:
|
Hello tinkof Only if you use a Simatic SD Card then you could prevent Data loss if you turn out the Power of the Panel and the Runtime still runs. look at this one: https://support.industry.siemens.com/cs/ww/en/view/95853895 Also you should activate the option Control Panel -> OP-> "Automatically repair file system errors on storage...." But if you have a not Siemens SD Card then you should deactivate the Runtime before you turn of the Power or use a UPS: https://support.industry.siemens.com/cs/de/en/view/21633613 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on