1/10/2017 7:25 AM | |
Joined: 12/22/2012 Last visit: 8/26/2025 Posts: 92 Rating:
|
hii friends i decided to download an empty project when i wake up tat his snowy morning to test what is going on. I connected only HMI to my pc now and at my previous tests. I got same problem. I just modify ip address at my config file only. Also there is a strange thing there are two accessible device to be online even my pc connected to only one HMI. I attached all tree online info about that devices. Maybe i need to modify something at the hmi side. Attachmentcapture.zip (291 Downloads) |
1/10/2017 7:38 AM | |
Joined: 12/22/2012 Last visit: 8/26/2025 Posts: 92 Rating:
|
this is the factory reset screenshot. I become online with HMI and can not reset it? |
1/10/2017 8:34 AM | |
Posts: 648 Rating:
|
Hey corkscrew2, did you check your transfer settings? Did you press the button "Transfer" in the Start Center of the RT-System? With best regards rh1990 |
Follow us on