1/10/2017 5:18 PM | |
Joined: 3/28/2015 Last visit: 5/15/2024 Posts: 721 Rating: (213) |
Hello, Perhaps the following topic might help: How do you backup/restore with a Comfort Panel? 1-It is not possible to open and process the backup file with WinCC (TIA Portal). The file can only be downloaded to the original or another panel of the same type with a restore procedure. 2-You should have the configuration file if you want to open or edit the program. |
Eng.Mohamed Ibrahim |
|
1/10/2017 6:06 PM | |
Joined: 1/15/2016 Last visit: 8/7/2023 Posts: 178 Rating: (4) |
Thank you very much. |
This contribution was helpful to1 thankful Users |
Follow us on