1/11/2017 4:21 PM | |
Posts: 31 Rating:
|
Can anyone help me? Its kinda urgent |
1/12/2017 9:49 AM | |
Posts: 648 Rating:
|
Dear Fabio, two points: 1) you can't make a project with OP17 in TIA-Portal. The product life cycle ended in year 2007. This device is not available in the hardware catalog. Only the OP series 70 and OP 170 series can be programmed. You need WinCC flexible 2008. 2) a direct migration from proTool two TIA Portal is not possible. First you have migrate to WinCC flexible (link). The you have to migrate from WinCC flexible to TIA WinCC (link). I give you the advertise to buy a new Panel. With best regards rh1990 |
1/12/2017 9:55 AM | |
Posts: 31 Rating:
|
Thanks for the reply! 1 - I know that,i am converting that HMI to a new version of HMI. 2 - I did that,i converted to WinCC and then to TIA Portal My only problem is that button cause i dont know if it is "set bit" or "set bit while key is pressed" cause in Pro Tools its says nothing about that and when i migrated the buttons were not well converted |
Follow us on