1/15/2017 3:47 PM | |
Posts: 10 Rating:
|
hi, how can i manually migrate uss_wpm from microwin to tia portal? Do i still need to worry about db_ptr? |
1/22/2017 7:28 PM | |
Posts: 5225 Rating:
|
You are migrating S7-200 to S7-1200. My guess is that this is for parameter writing. The instruction writes values to respective parameters on the drive. The pointers represent the address positions for values that are written via USS. My suggestion is - Do the converting of S7-200 to S7-1200, keeping the "black boxes" as unknown. Thereafter teach yourself how USS instructions in the S7-1200 works. A helpful and very detailed article can be found: Now you can code the insides of the "black box". |
Last edited by: William_B at: 1/22/2017 7:35:39 PMexpand a little more |
|
Follow us on