(0)| 1/26/2017 7:49 AM | |
|
Posts: 4620 Rating:
|
Hello Kbv, S7 200 Code? OP7 Code? Have you tried using ProSave? Because the problem are the keys and the messages (if you have in OP7), all is not resident in the PLC. So if you can make an Upload of the panel is easier and you have to find an OP7 with the same code, otherwise you have to rewrite the functions in the new panel and below is a list of such panels can be connected to S7 200. Which HMI components can you connect with S7-200 CPU and what ... Migration OP7 --> OP77 --> KP400 Good luck |
Last edited by: Ste39 at: 1/26/2017 7:58:58 AM |
|
This contribution was helpful to
|
|
Follow us on