2/11/2017 6:26 PM | |
Joined: 12/9/2010 Last visit: 10/8/2022 Posts: 623 Rating: (76) |
Hi iadapt, Can u attach screenshot ? FC can't be monitored if it is not called or called in error OBs. The RUN status at the bottom will not flash. |
If you like the comment, rate it (right top) or thank it (left bottom). |
|
This contribution was helpful to1 thankful Users |
2/11/2017 9:45 PM | |
Posts: 10 Rating: (0) |
Yes, I will post a pic in a few minutes. |
2/11/2017 10:02 PM | |
Posts: 10 Rating: (0) |
I have attached a picture of the code. |
2/12/2017 6:25 PM | |
Posts: 10 Rating: (0) |
Thank you I will try that. |
This contribution was helpful to1 thankful Users |
Follow us on