2/16/2017 9:40 AM | |
Joined: 12/18/2014 Last visit: 5/28/2024 Posts: 33118 Rating: (4088)
|
I have for you a UDF manufactured, and adjusted to the measuring range -100 to 400 bar, with a sensor 4-20mA. If you simulate it in the attached LSC file, please remember that the value displayed at the analog input is the units after the A / D converter. This means 4mA corresponds to 200 Units. AttachmentDummy.zip (57 Downloads) |
Follow us on