2/28/2017 3:06 PM | |
Posts: 25 Rating:
|
Hi, William_B,
Both of them are asynchronous to a PLC cycle. (Once I tried to use a tag set by an event of a button as an InOut param...) Regards |
Last edited by: zdej at: 2/28/2017 3:06:22 PM |
|
2/28/2017 3:09 PM | |
Posts: 5225 Rating:
|
..have a closer look at that example. |
Last edited by: William_B at: 2/28/2017 3:19:55 PMNOTE: Suggestion is only of academical significance. |
|
3/1/2017 3:07 AM | |
Joined: 3/16/2015 Last visit: 10/10/2021 Posts: 1250 Rating:
|
Thanks william, I greatly appreciate your feedback. I will re-read you reply again to let it sink in along with the entire thread as it has quite a few people sharing new and good ideas. I attached an example of what I mean and I apologize for all the undeclared tags as I had to slim down an existing project to make is small enough to upload. I am generally careful not add to much code or block calls to an interrupt as I understand it could have a detrimental effect on cycle time. Cheers Kal Attachmentkal_interrupt.zip (231 Downloads) |
Follow us on