3/24/2017 11:50 AM | |
Posts: 1 Rating:
|
Downloading the files works with above solution, but how to do this with a firmware version >= 4.2? Thanks. |
3/24/2017 8:02 PM | |
Joined: 9/16/2010 Last visit: 8/12/2024 Posts: 109 Rating:
|
Since firmware 4.2 it is a little bit tricky to download the datalog. I think the best way is using the program wget. The new since 4.2 is, that the download is only possible after login. So write a batchfile. The second line use the cookie for logincheck and downloads the datalogfile. All PC-Pathes and filenames (cookie, html, datalogfile) are of course arbitrary. The regular wget-path after the installation is "C:\Program Files (x86)\GnuWin32\bin\wget.exe". IP-Adr and dataLogFileName i think is clear.
See the Attachment. The forum dosn't akzept the content in the text. AttachmentDownload_DataLog.cmd.txt (934 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on