4/1/2017 1:50 PM | |
Posts: 5 Rating:
|
Hello! I'm newbie here and have problems to read modbus data to my Logo FS4. In my home I have couple of Logo 8 and one FS4. Data connections between Logos works fine but I'm no able to read HR registers from modbus devices. My FS4 have IP 192.168.1.4 and I try to read over MODBUS IP 192.168.1.8 HR 50544 (Containing 2 words, data type is S32, I think it's mean signed 32 bits) I tried to modify example of this thread to my project but no help :-/ Maybe somebody can help me? Best Recards: Toni ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 4/3/2017 10:26:03 AMNew subject after splitting |
|
4/1/2017 2:21 PM | |
Joined: 12/18/2014 Last visit: 7/26/2024 Posts: 33416 Rating:
|
Try the examble in attachment.
AttachmentModbus.zip (576 Downloads) |
Follow us on