4/10/2017 10:05 AM | |
Posts: 2826 Rating:
|
Hello. Arasan - you are going to create all sorts of chaos with that answer of yours.. even if it is just a typo. SOble - Have a look at: http://w3.siemens.com/mcms/programmable-logic-controller/en/basic-controller/s7-1200/cpu/Pages/Default.aspx?tabcardname=standard%20cpus Best to follow the directions from the first reply and read the PLC manual or place a PLC in the hardware configuration and read the documentation description of the hardware. Bye. |
This contribution was helpful to
2 thankful Users |
Follow us on