4/9/2017 1:26 AM | |
Joined: 4/3/2017 Last visit: 9/12/2024 Posts: 69 Rating: (1) |
He told me nothing.. Can you help please? |
4/9/2017 4:11 PM | |
Joined: 12/18/2014 Last visit: 11/7/2024 Posts: 34155 Rating: (4254)
|
For a master/master connection, use the client/server method. One LOGO! is the client, the other LOGO! the server. The client LOGO! requests data from the server LOGO!, the server LOGO! sends data according to request from the client LOGO!. Which of the two LOGO!s is the client is no matter and can be arbitrarily set by the user. In my example it is the LOGO! with the low IP address the client, it becomes the state of the inputs I1 and I2 to the server LOGO! And the client LOGO! Asks the state of the two inputs I1 and I2 of the server LOGO! from. The two inputs of the respective LOGO! switch in the other LOGO! the outputs. Setting up the client LOGO!: Setting up the server LOGO!: Simulation: Since all videos are too large for an attachment, I distribute the videos to several Posts. AttachmentClient-server.zip (377 Downloads) |
4/9/2017 4:17 PM | |
Joined: 12/18/2014 Last visit: 11/7/2024 Posts: 34155 Rating: (4254)
|
Here's the video "Client Connection.wmv".
AttachmentClient connection.wmv (336 Downloads) |
4/9/2017 4:18 PM | |
Joined: 12/18/2014 Last visit: 11/7/2024 Posts: 34155 Rating: (4254)
|
Here's the video "Server Connection.wmv".
AttachmentServer connection.wmv (349 Downloads) |
4/9/2017 4:19 PM | |
Joined: 12/18/2014 Last visit: 11/7/2024 Posts: 34155 Rating: (4254)
|
Here's the video "Simulation.wmv". AttachmentSimulation.wmv (325 Downloads) |
4/16/2017 8:40 AM | |
Joined: 12/18/2014 Last visit: 11/7/2024 Posts: 34155 Rating: (4254)
|
in attachment an example for sending a value from server to client.
AttachmentSend_value_from_server_to_client.zip (375 Downloads) |
5/2/2017 8:23 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4766 Rating: (122) |
New question published by luka31 is split to a separate thread with the subject LOGO OBA7, how to configure Logo App. Best regards |
Follow us on