5/7/2017 7:54 PM | |
Joined: 5/2/2017 Last visit: 10/17/2024 Posts: 14 Rating: (0) |
Greetings, When navigating the project after some time Hangup hole project... at this time following messages getting from "PMdiaganosis log file" 2017-05-07 17:24:52.024 PM(2120-2388) DoImplicitMigration, MigrateMCP File 2017-05-07 17:24:55.355 PM(2120-2388) *** !!! *** EXCEPTION CRedundancyState::throwIfFailed CRedundancyState::FindServers() hr(0x80004005) 2017-05-07 17:26:45.375 PM(2120-2388) CRTApplication::StartWinCCApplication CreateProcessAsUser failed for CAReportMergerX.exe with error 183: Cannot create a file when that file already exists. 2017-05-07 17:26:45.375 PM(2120-2388) CRTApplication::StartWinCCApplication GetFileAttributes of CAReportMergerX.exe failed 2017-05-07 17:26:45.375 PM(2120-2388) CRTApplication::StartWinCCApplication GetFileAttributes of CAReportMergerX.exe failed Why this problem coming, How can i solve this problem Please clarify any one.... thanks AttachmentWinCC log file.zip (41 Downloads) |
Follow us on