6/2/2017 8:11 PM | |
Joined: 3/8/2011 Last visit: 5/17/2023 Posts: 262 Rating: (20) |
Dear Aranel, I have a vb script to create the testdata folder in storage card as below Dim f, dtDateTime, sPath, sFolder1 Set f = CreateObject("FileCtl.FileSystem") sPath = "storage Card SD" sFolder1 = "TestData" 'Check to see if folder 1 structure exists, if not then create it If f.Dir("\" & sPath & "\" & sFolder1, 16) = "" Then f.MkDir "\" & sPath & "\" & sFolder1 ShowSystemAlarm "Storage Folder Main Structure Created" ElseIf f.Dir ("\" & sPath & "\" & sFolder1, 16) = sFolder1 Then 'ShowSystemAlarm "Storage Folder Main Structure Already Exists" End If Set f = Nothing I want to make some changes and test this script on my laptop so do i need to change the syntax for changing path. I am unable to create folder if i change the path . Do i have to use windows pc instructions ??? And also how to merge the line while writing data in excel?? ------------------------------------------------------------------------------------------ |
Last edited by: Dongerpure at: 6/2/2017 8:15:22 PMLast edited by: Min_Moderator at: 6/9/2017 4:33:40 PMNew subject after splitting If this post helped you, you may use the Rate-button |
|
Follow us on