6/8/2017 2:58 PM | |
Posts: 113 Rating: (1) |
Hello everyone, Is there any documentation about using neuronal network controller in step 7 or wincc? Also documentation about Fb 50, Fb 51? Best regards |
6/8/2017 3:33 PM | |
Posts: 8946 Rating: (999) |
Ask HER, she can tell you exactly. |
This contribution was helpful to1 thankful Users |
6/8/2017 4:43 PM | |
Joined: 9/27/2006 Last visit: 5/26/2024 Posts: 12257 Rating: (2668) |
Hello new-tech; Siemens offered a Neural Network design package as part of PCS 7, as an add-on. See the following attachment, specially page 3. The notice on page 3 comes from the Siemens Industry Mall, the electronic catalog for all things related to Siemens automation. It is always current. So the product is no longer offered officially, but can still be negotiated with a Siemens rep... Good luck. Here are links to the product information, if you care to look at more details: NeuroSystems - a Configuration Tool for Neuronal Networks NeuroSystems Version V5.0 Released for Delivery Hope this helps, Daniel Chartier Edit: FB50, FB51 are generic names for function blocks, they can be linked to a Siemens product, or a vendor's program, or even a programmer's design. We need more information before we can help you there. D.C. AttachmentNeural networks PCS 7.pdf (218 Downloads) |
Last edited by: dchartier at: 6/8/2017 4:45:54 PM |
|
This contribution was helpful to2 thankful Users |
6/9/2017 11:50 AM | |
Posts: 113 Rating: (1) |
Thank you so much for your help. About FB50 and FB51 as PID SELF TUNER, and is there any relationship between thise blocs and the neuronal network system? |
This contribution was helpful to1 thankful Users |
6/9/2017 6:30 PM | |
Joined: 9/27/2006 Last visit: 5/26/2024 Posts: 12257 Rating: (2668) |
Hello new-tech; If I remember well, the PID Self Tuner used an adaptive algorithm to iterate between different values of parameters for the standard PID FBs of S7 controllers.Neural networking techniques were not involved, as Jurgen pointed out. In any case, studying a manual of the PID Self Tuner should explain much: PID Self-Tuner - Siemens Support Hope this helps, Daniel Chartier |
6/10/2017 9:06 AM | |
Posts: 8946 Rating: (999) |
Some more Information about regulators with simatic equipment: https://www.amazon.de/Regeln-mit-SIMATIC-Praxisbuch-Prozessautomatisierung/dp/3895783404 |
Follow us on