6/27/2017 4:25 PM | |
Posts: 1 Rating: (0) |
Hi, I like to update a 1214C from version 4.X to 4.21 using a SD card, since customer don't have TIA installed on there computers. Is it the same procedure as with 2.X? BR Magnus ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 6/28/2017 2:24:46 PMNew subject after splitting |
|
6/28/2017 6:12 AM | |
Joined: 5/12/2006 Last visit: 10/2/2024 Posts: 22388 Rating: (3015) |
Hello, yes is the same. You can also perform a FW Update with SIMATIC Automation Tool. Regards Christoph |
This contribution was helpful to1 thankful Users |
Follow us on