8/4/2017 10:13 AM | |
Joined: 2/24/2015 Last visit: 1/25/2023 Posts: 306 Rating:
|
Hello. There is a computer with VirtualBox installed. In the settings of the virtual machine adapter - virtualbox host-only ethernet adapter. Host PC: Soft - Tia Portal v14 sp1 (Step 7 Prof + WinCC Prof) OS - Windows 10 IP - 192.168.33.2 Name - ES Guest PC: Soft - WinCC Runtime Prof v14 sp1 OS - Windows 7 IP - 192.168.33.10 Name - OS-SERVER I can not download project to a virtual machine. Computers do not see each other through the Simatic Shell. Ping IP address, ping computer name - OK. I can see each other's network folders. If I select "bridged adapter" in the settings of the virtual machine adapter, then everything works. But this requires an external switch / router. It would be interesting to try working through the virtualbox internal network. Instead of Virtualbox tried VMWare - the same story.
AttachmentVirtualbox.zip (174 Downloads) |
Follow us on