8/15/2017 8:21 PM | |
Joined: 9/27/2006 Last visit: 9/16/2025 Posts: 12409 Rating:
|
Hello sukhoi; From https://support.industry.siemens.com/cs/attachments/42122427/BA_CP-243-1_76.pdf?download=true The CP 243-1 provides the following functions: ● S7 communication… ● IT communication… ● Configuration: – Remote programming, configuration and diagnostics of an S7-200 system (for example program upload and download or status indications) via Industrial Ethernet and STEP 7 Micro/WIN 32… The usage and connection of the CP 243-1 is described in the following system manual, pages 220 and following): S7-200 Programmable Controller System Manual You setup connections for the CP 243-1 through the Set the PG/PC Interface dialog box, the same as for any communication interface for all S7 PLCs, as shown in the proposed pages. Hope this helps, Daniel Chartier |
Last edited by: Jen_Moderator at: 8/22/2017 12:31:09 PMInserted right links. |
|
Follow us on