(0)| 8/10/2017 9:30 AM | |
|
Posts: 6 Rating:
|
Hi Everyone, I want to transfer PLC Program from old S7-200 PLC(having orignal program code in Volatile memory) to new S7-200 PLC using memory cartridge? And old S7-200 PLC not having memory cartridge so if i install new memory cartridge in old CPU then can i transfer the program from old PLC to another using memory cartridge. I want to do this to backup Original program, data and system blocks from PLC because program uploading using PPI PC adapter disabled by programmer And my concern is that when we install memory cartridge in PLC then on power up contents of Memory cartridge are copied to internal memory of PLC so when i will install new memory cartridge in my old PLC then how it will behave on power up? Will it clear the internal PLC memory? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 8/10/2017 3:17:27 PMNew subject after splitting |
|