6/19/2008 10:40 PM | |
Posts: 2661 Rating: (279) |
After creating a user, when you activate WinCC runtime, the login window appears automatically. For this window to appear, at least one user should be added in the User Administration. The user can log off by clicking on the key symbol in the keyset or clicking the username in the top right corner. See attachment. This link describes how to block/enable key combinations. This is a very special case. Blocking key combinations can be very useful, for example if you want to prevent the plant operators from accessing Windows. AttachmentDokument1.pdf (160 Downloads) |
6/20/2008 5:18 PM | |
Posts: 2661 Rating: (279) |
Jasner: Sorry about that! I never used "native" WinCC and did not fully comprehend the limitations! The following FAQ should help solve your problem: How can you implement login/logout via a button in a picture? |
Last edited by: Phantom75 at: 6/20/2008 5:24 PMAdded info about logout. |
|
Follow us on