10/13/2017 12:05 AM | |
Joined: 10/5/2016 Last visit: 9/12/2022 Posts: 236 Rating: (7) |
Hello community, Who knows how to change icon of Alarm Control User Defined Button on the Toolbar ? See attach... |
10/13/2017 8:56 AM | |
Joined: 11/4/2011 Last visit: 12/8/2023 Posts: 253 Rating: (53) |
Hi. You are lucky. Here is a complete solution. Remove ".txt" in the file name and run this SFX-archive. It will ask/warn you that it is going to copy some files to some folder — just click OK. You may copy the folder path from that dialogue and open the folder after this import procedure. Then in Graphics Designer go to Properties of Alarm Control and change Style property to the newly created SlgButtons. Done. AttachmentSlgButtons Control Skin.exe.txt (222 Downloads) |
Follow us on