6/9/2009 11:05 AM | |
Posts: 2 Rating: (0) |
Hi All, Can I use "505-cp2572" to communicate with 3rd party PLC, like Mitsubishi Q-series PLC by ethernet. Please advice if you have any informatiom. Thanks |
6/9/2009 12:55 PM | |
Posts: 510 Rating: (117)
|
I am unfamiliar with the Mitsubishi PLC. If the Mitsubishi PLC supports TCP Send Receive functions you should be able to pass information back and forth. Chapter 4 of the attached manual has application code on setting up the send receive between two CP2572 modules. Send from one and receive from the other. You can use this as a guide for setting up the Mitsubishi if it supports Send receive functions billwest Attachment06200146-025.pdf (1126 Downloads) |
5/10/2012 10:05 AM | |
Posts: 3 Rating: (0) |
fixed buffer comms is the best method, i have this working and is reliable |
Follow us on