11/30/2017 5:03 AM | |
Joined: 1/30/2013 Last visit: 10/1/2022 Posts: 13 Rating: (1) |
Project file size gets bigger by a lot and deleting all the devices in the project will even increase the file size!
I don't know what is causing this but I have an old project (named V1) 114MB in size, then I deleted all devices and saved it as V2. The project size is now 115MB. I DELETED ALL INSIDE THIS PROJECT BUT IT INCREASED ITS FILE SIZE! Then I tried to create a new project named V3, copied all the devices from V1 to this new project. Reconnected the Profinet connections, compiled all, then saved it. I didn't touch any of the hardware settings and code. The new project size is 22MB! I tested the code and it worked as it should! How could V1 get so big when it is originally 22MB worth of code? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/30/2017 1:01:14 PMNew subject after splitting |
|
11/30/2017 4:21 PM | |
Joined: 7/7/2010 Last visit: 11/19/2024 Posts: 15406 Rating: (2446)
|
I am told a simple way to accomplish the "unbloating" of a portal project is to archive it, then restore from archive. It only archives what is needed, without any undo possibilities or whatever else they store in there. I too wonder why the projects get so large.
|
science guy |
|
11/30/2017 4:43 PM | |
Joined: 4/20/2007 Last visit: 11/7/2024 Posts: 728 Rating: (43) |
I have also noticed that upgrading to V14 reduces the size of the project significantly! Less than 50%! |
Follow us on