(0)| 1/2/2018 3:53 PM | |
|
Posts: 26 Rating:
|
@Alex Mol Hello, Can anybody suggest a similar solution with latching relay ABB E 251-230 (2CSM111000R0201) alike? Thanks ------------------------------------------------------------------------------------------ |
Last edited by: ptd22 at: 1/2/2018 3:56:14 PMLast edited by: CS Moderator at: 1/4/2018 11:35:52 AMNew subject after splitting |
|
| 1/5/2018 2:53 AM | |
|
Joined: 9/2/2008 Last visit: 8/3/2025 Posts: 191 Rating:
|
Well, yes and no. The output from the PLC can be parallel with the push button to the ABB relay, but inside the PLC you don't need a flip-flop function. I don't know how Weintek's HMI software is working, but with Siemens you can give an 'inverse bit' property to your HMI button. This will invert the selected PLC's output bit directly when someone pushes this HMI button. So all together you don't need what is mentioned in this post: Ladder logic to start/stop motor using only one button Regards, Alex |
|
Problems don't exist, only challenges. |
|
Follow us on