2/6/2018 11:44 AM | |
Joined: 12/4/2014 Last visit: 2/17/2022 Posts: 3 Rating: (0) |
Ok. I have CPU 1211C, which is connected to SATO WR4 printer. Lets say I want to send "reprint" command, which is ESC+C. Is it enough to send data like on the picture DB.jpg? Here is a manual and the "reprint" command is on page 182: I need to prepare the code before I can test on the factory site... |
Follow us on