7/20/2008 4:57 AM | |
Posts: 2661 Rating: (279) |
First you need to do settings as described in the following FAQ: How do you lock typical Windows key combinations in WinCC V6? AttachmentDokument1.pdf (294 Downloads) |
7/29/2008 4:11 PM | |
Posts: 2661 Rating: (279) |
Hi Daniele, In WinCC explorer the "User Administrator" editor. Tryas I suggested and it'll work. Regards, Phantom75 |
8/1/2008 5:34 PM | |
Posts: 7 Rating: (0) |
Hi Phantom, |
8/1/2008 7:18 PM | |
Posts: 2661 Rating: (279) |
Hallo Daniele, It's my fault again! I failed to recognize that you are using native WinCC and not PCS7 WinCC! The settings I described were for the PCS7 created WinCC project. See the attachment. You'll see the user admin as shown in first picture. Now my question is, do you have @buttons12.pdl in your project? If you have,then enable/disable level 3 (Process controlling). If you do not have @buttons12.pdl, you'll have to program the functionality as shown in the attachment. Hope this time it'll work. Regards, Phantom AttachmentUserAdmin_NativeCC.pdf (239 Downloads) |
Follow us on