3/1/2018 10:58 AM | |
Posts: 80 Rating: (1) |
Hello, I can not connect to micromaster 440. I use the usb cable on rs232. And the regulator connects to the profibus. Can help
|
3/1/2018 11:09 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Please refer attached FAQ.
AttachmentUSB_RS232_Adapter_en_V1_2[1].pdf (437 Downloads) |
This contribution was helpful to1 thankful Users |
3/1/2018 11:41 AM | |
Posts: 80 Rating: (1) |
Everything is set up but will not connect Which parameters should be set on the micromaster? |
Last edited by: muha_mag at: 3/1/2018 11:43:53 AM |
|
3/1/2018 12:27 PM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello, My PG/PC has only USB com-ports. How I can get online with my drive? |
3/1/2018 3:27 PM | |
Posts: 80 Rating: (1) |
everything is ok but it still can not connect. Is it a problem if I connect via PROFIBUS, and I do not have another micromaster port |
3/2/2018 10:53 AM | |
Posts: 80 Rating: (1) |
Hi, I thought I set everything as stated in the previous manual but it is not good again. I use STARTER, OS win10, the cable is a usb toRS232 converter
|
3/2/2018 11:30 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Please refer Uploading and downloading drive parameters of a MICROMASTER 4xx using STARTER (1,5 MB) . Though the example is for MM420, it is same for MM440. You need SINAMICS MICROMASTER STARTER V4.5 SP1 and additive SSPs since your PC OS is windows 10, which you can download from below link. Vol_1_STARTER_V45_SP1_Program_G110_G120.zip (1,8 GB) Please refer mm4_online_starter_eng.ppt (629,0 KB) which will help you to set communication parameters. HTH. |
Last edited by: Jen_Moderator at: 3/2/2018 11:38:02 AMOptimized links. |
|
Follow us on