3/5/2018 3:41 PM | |
Joined: 9/28/2012 Last visit: 11/30/2023 Posts: 75 Rating: (3) |
For everybody who want to use the 1214 V4.X plc to send emails, i have made a ready to use email program including email accounts setup and test mail. U have only to change some minor items on the IP adressing site to get it working on your plc, sps. Please first read the "read this first" file. and don't change accounts so it stays working. if you are in company, first check with your IT department which emailport is open to the internet, or let a port set open to the internet. for example port 25 or 2525 or 587. first unzip and then in tia do retrieve (in menu tab project-retrieve) have fun, Naaltje I have updated the program a bit. I added some explanation in the program with tekst, added diagnose to see what the block is doing, in terms of, busy, done, error and the last error will be saved, so you can find easier what went wrong. concerning logging in on the gmail account. gmail is not letting you in due to security reasons, but you can solve this by changing the email adress in one of your own. i mean the "to" adress. As far as i know smtp2go is letting you in so do not change this one. First start to get it working and later you can change everything step by step. If you have remarks please let me know, also if you have used it succecfully. again first unzip and then in tia do retrieve (in menu tab project-retrieve) have fun, Naaltje Attachmentemail-plc-1200-V14_2.zip (104 Downloads) |
Last edited by: Naaltje at: 5/3/2018 10:22:31 AMLast edited by: Naaltje at: 5/3/2018 10:24:18 AM |
|
This contribution was helpful to4 thankful Users |
Follow us on