3/30/2018 12:56 AM | |
Posts: 4 Rating: (0) |
how to give a modbus address of a variable for example m0.0 or mw100 in s7-1200 . thank you.. |
3/30/2018 11:36 AM | |
Posts: 2826 Rating: (684) |
Hello.
Assuming the S7-1200 is the slave: The "Modbus slave" instruction maps the Modbus address to relevant PLC memory. this is done in block sizes and not single bits. Have a look at the example: Regards. |
Follow us on