6/11/2018 11:32 AM | |
Joined: 12/18/2014 Last visit: 7/11/2024 Posts: 33328 Rating:
|
Are a code with 4 numbers enough? |
This contribution was helpful to
1 thankful Users |
6/11/2018 2:04 PM | |
Joined: 5/13/2016 Last visit: 1/15/2022 Posts: 66 Rating:
|
Maybe I'm wrong, however I think you're asking how to make a push button instead of a switch? Seems like it's not possible looking at this: https://support.industry.siemens.com/tf/ww/en/posts/logo-8-2/185641/?page=0&pageSize=10 However ixo65 seemed to have a work around. |
This contribution was helpful to
1 thankful Users |
6/11/2018 5:00 PM | |
Joined: 12/18/2014 Last visit: 7/11/2024 Posts: 33328 Rating:
|
Here is a complete solution for a 4-digit code. The code for unlocking is 3690. Arming of the system is done via "*" and then within one second "#".
AttachmentCode_lock.zip (149 Downloads) |
Last edited by: ixo65 at: 6/11/2018 7:45:04 PMbetter version of LSC file |
|
This contribution was helpful to
3 thankful Users |
6/12/2018 5:18 AM | |
Joined: 12/18/2014 Last visit: 7/11/2024 Posts: 33328 Rating:
|
Here is another, resource-friendly version. The password can be set from 2 to 999998. In the program suggestion is the password 618724. The ON parameter of the counter corresponds to the password, the OFF parameter is password + 1. The alarm system would be locked when entering 0 in the password entry field. AttachmentCode_lock_V2.zip (126 Downloads) |
This contribution was helpful to
2 thankful Users |
Follow us on