7/27/2018 3:10 PM | |
Joined: 3/2/2007 Last visit: 7/4/2024 Posts: 932 Rating: (5) |
Kindly, we need to wire a solid state relay to a digital output on connector X101 of the below masterdrive inverter. It is mentioned in the manuals that the digital output can support 20 mA loads maximum. So, can we us the following solid state relay for it? Fotek SSR-10DD http://www.fotek.com.hk/solid/SSR-3.htm http://www.ekt2.com/pdf/42_SOLID_STATE_SSR-10DD.pdf ***SPARE PART*** SIMOVERT MASTERDRIVES MOTION CONTROL - PERFORMANCE 2 INVERTER COMPACT PLUS UNIT, IP20 DC 510V - 650V, 10.2A NOMINAL POWER RATING: 4.0 KW DOCUMENTATION ON CD ***SPARE PART*** C33=Measuring transducer for Resolver with pulse encoder simulation SBR2 Slot C ***Spare part*** G91=Communication module PROFIBUS CBP2 inserted at Slot A |
... thank you ... |
|
Follow us on