3/23/2006 11:28 AM | |
Posts: 21 Rating: (0) |
Hello, In a project I use an Alarm window in my template. In that alarm window I use the Ack-button. Is it possible to link a tag (bool)to that button? Thx |
3/23/2006 2:34 PM | |
Posts: 3149 Rating: (171)
|
Hi Imele, unfortunately you cannot use the button on the template.... Perhaps these FAQs can help: http://support.automation.siemens.com/WW/view/en/22531596 http://support.automation.siemens.com/WW/view/en/22411008 this should work with WinCC flexible as well: http://support.automation.siemens.com/WW/view/en/22778796 Nemo |
Follow us on