8/14/2018 9:30 AM | |
Joined: 7/30/2018 Last visit: 6/18/2024 Posts: 13 Rating: (0) |
I have not build a system yet but are in the design stage. Want to use multiple Logo's in my house all connected to LAN. What happens if you use a network input from another Logo and this one is not accessible as for example Logo defect/off or LAN down .. would this trigger an error ? This way we can create a dummy circuit just to detect if there is a problem. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 8/14/2018 12:01:54 PMNew subject after splitting |
|
Follow us on