8/16/2018 1:09 PM | |
Joined: 11/9/2017 Last visit: 6/2/2023 Posts: 44 Rating: (0) |
When I choose legacy Hard Drive and press Enter I get No bootable device -- insert boot disk and press any key |
8/16/2018 1:25 PM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2985) |
and is you select efi and press esc after that? |
8/16/2018 1:36 PM | |
Joined: 11/9/2017 Last visit: 6/2/2023 Posts: 44 Rating: (0) |
then Windows have been loading normally Why ESC? I choose and press Enter. ESC after that not needed |
8/16/2018 3:42 PM | |
Joined: 11/9/2017 Last visit: 6/2/2023 Posts: 44 Rating: (0) |
In Bios are many menu for example [snip] If I choose Boot from file I can find from explorer boot folder and press .efi file [snip] Further is showed this screen [snip] If I press C then is loaded [snip] If Enter then [snip] Further I can't do something more AttachmentImages.zip (658 Downloads) |
Last edited by: Jen_Moderator at: 8/17/2018 8:24:33 AMAdded files as an attachment. |
|
Follow us on