4/25/2017 8:10 PM | |
Joined: 9/2/2008 Last visit: 6/30/2024 Posts: 191 Rating: (43) |
Hello Dan, You were right. A measurement for two hours at a minimum cycle time of 75ms gave me a -40s deviation. For me this part is clear. At this moment (and for the last couple of days) I'm testing your STOPWATCH in several ways. Some unexplained things I've seen so far. Nothing to worry about on your side. The results I will post in your RUNTIME topic. Regards, |
Problems don't exist, only challenges. |
|
5/5/2017 6:21 PM | |
Posts: 2826 Rating: (685) |
Hello. The following attachment contains the latest version of code that was shared earlier. For more detail see also: Regards. AttachmentPLC_CYCLE_V5.zip (424 Downloads) |
Follow us on