(0)| 10/9/2018 12:44 PM | |
|
Joined: 12/12/2016 Last visit: 12/11/2025 Posts: 640 Rating:
|
Hello, Does it only happen when you use the DI nodes? If yes, maybe you could try these nodes instead. It would also be interesting to see if node-red actually crashes or just freezes for a minute. You can run the command
in putty to see if the node-red process is still running. If a flow is causing the problem you can also kill the process, delete the flow like in this post. And restart node red with:
Kind regards! |
Follow us on