5/30/2011 8:18 PM | |
Joined: 4/20/2010 Last visit: 3/29/2024 Posts: 38 Rating: (5) |
Hi again ! Well, bad news, I've just had a crash again So, here are the two reports : First, extract from the file S7KAFAPX.RPT located in this directory : C:\Program Files\Siemens\Step7\S7tmp //===================================================== 05/30/2011 21:06:06 Exception code: C0000005 ACCESS_VIOLATION Fault address: 4C0B3A4A 01:000B2A4A C:\Program Files\Siemens\Step7\S7BIN\OT01600603AS.dll Registers: EAX:00000032 EBX:00000000 ECX:09419F38 EDX:00000002 ESI:025F3B58 EDI:0000E718 CS:EIP:001B:4C0B3A4A SS:ESP:0023:0022F9DC EBP:0022FB74 DS:0023 ES:0023 FS:003B GS:0000 Flags:00010246 Call stack: Address Frame Logical addr Module 4C0B3A4A 0022FB74 0001:000B2A4A C:\Program Files\Siemens\Step7\S7BIN\OT01600603AS.dll 73D21F5F 0022FBF8 0001:00000F5F C:\WINDOWS\system32\MFC42.DLL 73D21B07 0022FC18 0001:00000B07 C:\WINDOWS\system32\MFC42.DLL 73D228F1 0022FC38 0001:000018F1 C:\WINDOWS\system32\MFC42.DLL 73D21A78 0022FC98 0001:00000A78 C:\WINDOWS\system32\MFC42.DLL 73D219D0 0022FCB8 0001:000009D0 C:\WINDOWS\system32\MFC42.DLL 73DAE47C 0022FCE4 0001:0008D47C C:\WINDOWS\system32\MFC42.DLL 7E398734 0022FD10 0001:00007734 C:\WINDOWS\system32\USER32.dll 7E398816 0022FD78 0001:00007816 C:\WINDOWS\system32\USER32.dll 7E3989CD 0022FDD8 0001:000079CD C:\WINDOWS\system32\USER32.dll 7E398A10 0022FDE8 0001:00007A10 C:\WINDOWS\system32\USER32.dll 7E3A74FF 0022FE0C 0001:000164FF C:\WINDOWS\system32\USER32.dll 7E3BC6D3 0022FE2C 0001:0002B6D3 C:\WINDOWS\system32\USER32.dll 73D35202 0022FE9C 0001:00014202 C:\WINDOWS\system32\MFC42.DLL 005173C4 0064FA84 0001:001163C4 C:\Program Files\Siemens\Step7\S7SKA\S7KAFAPX.EXE 00000200 00230448 0000:00000000 And attached, the report automatically sent through Windows crash report If someone has any additional info, please inform, I'll appreciate ! Seb Attachment7cf0_appcompat.zip (330 Downloads) |
6/2/2011 6:49 PM | |
Posts: 947 Rating: (45) |
hello |
6/15/2011 11:18 AM | |
Joined: 4/24/2006 Last visit: 5/31/2024 Posts: 8664 Rating: (1154) |
Hello, Perhaps this link is usefull: how can you completely uninstall STEP 7 including all the software packages? Best regards, Wizard |
This contribution was helpful to2 thankful Users |
Follow us on