1/16/2018 6:38 AM | |
Joined: 12/18/2014 Last visit: 9/26/2024 Posts: 33840 Rating: (4206)
|
Now also on the english Product Support: Firmware update V2.1 for LOGO! CMR2020 (6GK7142-7BX00-0AX0) and LOGO! CMR2040 (6GK7142-7EX00-0AX0) The LOGO! CMR2020 and LOGO! CMR2040 modules are scheduled to be delivered with a new hardware product version 2 and a new firmware V2.1 as of late January 2018. The firmware V2.1 contains new functions and product enhancements. This update contains safety-relevant changes which enhance robustness against possible attacks. We therefore recommend that you update the firmware. The firmware is now available for download free of charge. The LOGO! CMR2020 and LOGO! CMR2040 with FW V1.x or V2.x that are already in use can be updated via the Web Based Management (WBM). 1. Functional enhancements
2. Product enhancements
|
This contribution was helpful to2 thankful Users |
8/7/2018 4:09 PM | |
Posts: 1 Rating: (0) |
It will be very very useful include ca certificate for VPN certificate because you can not use for OpenVPN in a iPhone |
12/21/2018 6:39 PM | |
Joined: 6/29/2018 Last visit: 11/28/2023 Posts: 57 Rating: (2) |
The above link doesn't work anymore. where can I download the latest firmware update? |
12/21/2018 6:45 PM | |
Joined: 12/18/2014 Last visit: 9/26/2024 Posts: 33840 Rating: (4206)
|
There's a newer firmware update. Take a look here: |
This contribution was helpful to2 thankful Users |
Follow us on