10/20/2018 1:23 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872)
|
Hello SIM2000, If you had mentioned your CCU MLFB number it would have helped to understand your system. I understood below points; please correct me if I am wrong. You want to reload NC & PLC arc files; here I presume your system is not operational. Main problems are, you do not know, whether it is with PCU 20 or 50 or MMC type. Second problem is, your system HMI is non-Siemens i.e. third party, as such standard data restoring procedures are not applicable in your case. Now the option left is you can reload back up directly in NC (memory) card, i.e. on PCMCIA card which is installed on CCU. For this you need SINUCOPY-FFS software on external PG/PC. Software & hardware requirement of external PC/Laptop is - OS Windows 95/ Windows NT, with PCMCIA drivers - PCMCIA card slot types II flash CSM PCJB (only for cards up to max 4 GB). When you have external PC with complete hardware & software, plug in PCMCIA (PC card) in slot & open SINUCOPY-FFS software, under FFS area, check if it has .arc files & replace those with the files you have as back up. BE CAREFUL ANY WRONG INSTRUNCTION MAY DELETE SYSTEM SOFTWARE FILE. Insert the card in system & switch ON the power, during power ON state files from NC card must get loaded in DRAM. HTH. |
10/20/2018 8:00 PM | |
Posts: 11 Rating: (0) |
yes dear. you are correct .my HMI IS NOT SIEMENS and it is not stranded industry i try to connect my display port with my Laptop with OS Windows 7 professional via RS232 cable and (winpcin) program and i reload the NC.ARC FILE = backup file. after finish . nothing happen ...................................................................................................................................................... now you correct me please what if i do a copy of NC.ARC = (BACKUP FILE) to the PCMCIA card by my Laptop with OS Windows 7 professional and then plunged it in to the ccu810 slot and set the s3 to 3 = see the attachment here is this what you want to explain to me or not note* my sinumerik is 810 D CPU 810DE CCU1 SOFTWARE VERS 7.4 IP 6FC5410-0AY01-0AA0 PLC IS S7-300 please advice and thank you very much |
Last edited by: SIM2000 at: 10/20/2018 8:27:14 PMLast edited by: SIM2000 at: 10/20/2018 8:48:00 PM |
|
Follow us on