12/24/2018 6:31 AM | |
Joined: 6/2/2010 Last visit: 10/1/2024 Posts: 41 Rating: (0) |
Hi, i am using CP341 to communicate with an Eurotherm P116. I am running the blocks and getting only TX on my cp. I am not so sure about the cables too and since i am making them myself, i need some assistance in making the 11 pin connector itself. The Eurotherm devices respond to a laptop running modbus communications, but do not to the CP. I am at my wits end trying to successfully diagnose the problem. Kindly help ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/25/2018 1:05:41 PMNew subject after splitting |
|
Follow us on