1/9/2019 3:59 PM | |
Joined: 5/27/2015 Last visit: 7/25/2024 Posts: 60 Rating: (27) |
Hi Could you give the exact version information? Regarding to the compatibility tool it should work, but it depends which Updates / Hotfixes are installed. If you have the latest updates it should work fine. Also there were some incompatibilities with some Windows 10 builds which also required the latest Service Packs and Updates. You can find the information to the compatibility under the following link: https://support.industry.siemens.com/cs/ww/en/view/64847781 Best regards |
Follow us on