1/17/2019 7:11 AM | |
Joined: 7/20/2015 Last visit: 9/26/2024 Posts: 154 Rating: (27) |
Hello All Software Details Wincc 7.0 Sp3+upd1 Simatic Net PC software v8.1 + SP2 I am doing wincc virtualization, And I have taken backup from physical wincc server and past in virtual server. I have moved all named connection tags on TCP/IP connection and I want to use software redundancy from Create connection redundancy (Because of redundant PLC)option which is generally available in dynamic wizard. But when I open dynamic wizard in my existing project in virtual machine I am not able to see create connection redundancy option. But when I create a new dummy project in same system and check create connection redundancy option in dynamic wizard its available. Detailed problem attached with this post. Anyone can help me why this is happening. Regards Sandeep Bakoliya AttachmentRedundancy Error.docx (299 Downloads) |
Last edited by: Sandeep Bakoliya at: 1/17/2019 7:55:52 AMRegards |
|
Follow us on