2/6/2019 1:07 PM | |
Posts: 2 Rating: (0) |
Is the problem solved ? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 2/12/2019 9:21:04 AMNew subject after splitting |
|
2/11/2019 11:57 AM | |
Posts: 2 Rating: (0) |
Hi8Noodles , I have some temperature sensors connected to work in MODBUS RTU mode and I want to read process values in WinCC Advanced v15_1 . For this purpose i am using (MOXA) Mgate MB 3170 gateway. Also I have configured WinCC for MODBUS TCP/IP protocol. The problem is that I am not getting continuos communication in WinCC. I used Siemens Sentron Powermanager software to verify communication, there I am getting 100% communication.
|
Last edited by: Mehmet Genca at: 2/11/2019 11:57:36 AMLast edited by: Mehmet Genca at: 2/11/2019 12:00:25 PM |
|
Follow us on