2/13/2019 3:05 PM | |
Joined: 6/16/2016 Last visit: 3/16/2024 Posts: 12 Rating: (0) |
Hello Wizard Could you please explain how can i change the number of static connections in the properties of the PLC ? I have the error code 4116 in the log file , although the rack/slot numbers are correct and they belong to the CPU414 - 3DP . The OS is windows XP , the Simatic Manager is V5.5 SP2 , and the Wincc V7.0 SP3 are installed respectively. I attached the online of module information Waiting your kind reply Regard Firas Al Khasha ------------------------------------------------------------------------------------------ |
Last edited by: AL KHASHAB at: 2/13/2019 4:41:52 PMLast edited by: Jen_Moderator at: 2/14/2019 11:09:16 AMNew subject after splitting |
|
2/14/2019 11:11 AM | |
Joined: 6/19/2017 Last visit: 6/7/2024 Posts: 8156 Rating: (165) |
Closed cause question posted twice. The second thread with the subject How can change the number of static connections in the properties of the PLC ? WinCC error 4116 is published within the conference SIMATIC WinCC. Best regards Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on