2/13/2019 1:23 PM | |
Joined: 6/16/2016 Last visit: 3/16/2024 Posts: 12 Rating: (0) |
Dear Mr. Berghof Could you please explain how can i change the number of static connections in the properties of the PLC ? I have the error code 4116 in the log file , although the rack/slot numbers are correct and they belong to the CPU414 - 3DP . The OS is windows XP , the Simatic Manager is V5.5 SP2 , and the Wincc V7.0 SP3 are installed respectively. I attached the online of module information Waiting your kind reply Regard Firas Al Khashab ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 2/14/2019 10:57:10 AMNew subject after splitting |
|
2/15/2019 1:43 PM | |
Joined: 6/16/2016 Last visit: 3/16/2024 Posts: 12 Rating: (0) |
Hello dchartier I attached S7 300 CPU Properties for one of the projects i have . Regard Firas Al Khashab |
Follow us on