2/21/2019 7:14 AM | |
Joined: 9/30/2016 Last visit: 5/23/2024 Posts: 912 Rating: (6) |
Hello Georg, Thank you for answering. Please also see the screenshots. I am not sure if it matters but our system is NOT a PCS7. It is an integrated project with S7 classic and WinCC 7.4 (in some other cases WinCC 7.0) handled in the Simatic Manager. I have (a long time ago) tried handling a WinCC system with 2 WinCC servers and a permanent Engineering WinCC (so that is actually a redundant system built with 3 WinCC servers) but that was a different philosophy where this system was handling several minor machines. In this present system there is only one WinCC server. What I was requesting help with was the partial download and what I failed to remember was that I actually need to go under PLC > Download even though I am downloading a single modified display. I have heard I need to do it some what differen for a full download but I will make a new thread for that.
AttachmentWCCDL.zip (43 Downloads) |
Follow us on