(0)| 3/28/2019 5:00 AM | |
|
Posts: 5 Rating:
|
HI DJ_1 My project is on Modbus RTU communication using S7200 Smart onboard port plus the Modbus RTU network formed by Communication board. Sample program for following configurations required. 1) Both ports acting as Master & Master 2) 1 port as Master & 1 port as Slave 3) Both pots acting as Slave & Slave Per PLC 10 packets of bool, byte, word, double word, real, string to exchanged on Modbus RTU and performance to be checked and along with function codes. With the above data exchange, how many slaves would be successfully connected per PLC. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/28/2019 2:12:12 PMNew subject after splitting |
|
Follow us on